LM Host Id and Composite Host ID for Virtual Server

2021-10-07T00:01:51Z

Summary


Details

Customer needs to move their RealNC license over to a new server. The new server is a Windows 2016 based virtual machine.
 
How should customer provide the LM Host Id and Composite Host ID for the Virtual Machine? 



Solution

The LM Host ID is the Physical address of the machine, as seen in the command "ipconfig /all". 

RealNC only uses this value, as it works with the old style Tecnomatix licensing. 

Run the RealNC installer, and only install the license server by selecting that from the RealNC installation selector. 

This will also include a file - "ugs_composite.exe". 

Run this in a CMD prompt shell, it will return the Composite ID. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 2012_R2
Product: TECNOMATIX
Application: REALNC
Version: V8.6.X
Function: LICENSING

Ref: 001-9606219

KB Article ID# PL8015913

Contents

SummaryDetails

Associated Components