Solid Edge 2019 - Maintenance Pack 10 Announcement

2021-10-07T00:10:02Z

Summary


Details

October 1, 2019
 
Dear Solid Edge Customer: 
 
Solid Edge 2019 Maintenance Pack 10 is now available for download.
 
Sincerely,
The Solid Edge Team 
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Solid Edge 2019 MP10
Version: 219.00.10.02
 
================
Download Location:
================
 
Solid Edge 2019 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
============================================
This Maintenance Pack addresses the following PRs:
============================================
 
===General===
PR 9562441: Cannot open some ST5 files
PR 9282767: KeyShot for SE doesn't work properly with subscription/cloud license file
PR 9562847: File open in SE can be released from Design Manager
 
===Assembly===
PR 9539217: After creating a system library, the .asm has double relations 
PR 9539393: Strange faces in KeyShot when converting from Solid Edge 
PR 9545353: Relationship is not created after inserting a component via drag and drop
PR 9576054: Assembly relations are not be placed with the assemble command bar
 
===Draft===
PR 9553058: Solid Edge Draft Crash when a small value is in custom props
PR 9556161: Reproducible Crash, when pasting text from a PDF file into a Text Box 
PR 9522862: Get the length of weld seam in Draft is incorrect
 
===Part/Profile/Sheetmetal===
PR 9070876: Propagate face colors during Boolean subtract of part copy
 
===Teamcenter Integration for Solid Edge===
PR 9506964: Release Status icons in File Properties do not match other places 
Shrinath - PR 9544573: Solid Edge 2019 crashed 2 times.
Shrinath - PR 9544658: Unexpected Attribute Mapping call while opening an Assembly on SESE 
PR 8428611: Download linked documents causes all FOP members to be downloaded to cache
 
===Translators===
PR 9388932: Open Parasolid assembly, multi-body all is not Design Body
PR 9539136: Incorrect use of a comma in the formula field after opening an STL file.
 

SFB-SOLID_EDGE-8015790
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8015790

Contents

SummaryDetails

Associated Components