Details
Last_mod_date is different between assembly data set and BOMViewRevision.
Solution
This is working as designed in ST9 (also in lower version than ST9).
The file upload process happens in two steps in code.
1.First it creates BOM
2.Then it uploads the dataset.
The time difference depends on the size of the BOM and the connectivity to the database.
Hence there is a difference of xxx seconds between Last_mod_date of assembly data set and Last_mod_date of BOMViewRevision.
It vary by seconds depending on the size of BOM
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP19
Function: SEEC
Ref: 002-8015775