TC10 / NX12 - monolithic JT file name is not ItemId_RevisionID.jt

2021-10-06T23:27:29Z

Summary


Details

When creating monolithic jt's of assemblies and stored in the Teamcenter (TC10) with ugtopv.exe, the generated JT file has the display name of the NX assembly as its name.

For the monolithic JTs generated with the same settings under NX10, the file name is formed from the item-id to an underscore and the revision-id.

Solution

Add the following parameters to the tess.config to have the same behaviour from NX10 in NX12:

appendItemName = false
configureFileName = true
appendTCIdentifiers = "UNIQUE_ITEM_IDENTIFIERS"

Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1507
Product: NX
Application: TRANSLATOR
Version: V12.0.2
Function: NX_JT

Ref: 001-9581315

KB Article ID# PL8015769

Contents

SummaryDetails

Associated Components