Modify released file without having to create a new revision

2021-10-06T23:56:16Z

Summary


Details

Is it possible to make modifications to released Solid Edge files without having to create a new revision of the file?

Solution

If a file is released then the file is read only.

Once a file is marked as released it is then not possible make any modifications to that file.

Once a file is released then the standard workflow should be to create a new revision of the that file to then make the desired changes.  This is the accepted practice for all drafting standards.  Additionally, in some industries such as medical and aerospace, it may be a legal requirement to not change data once the file has been released.

Therefore, if the customer has omitted information from a released file then theoretically the customer should create a new revision to add that missing information.  After all, it is possible that in the process of making what appears to be a simple change that then something inadvertently changes without the user being aware of it.

However, it is also understood that sometimes a customer may not want a new revision for a simple clerical type error.  We do provide a mechanism to allow the modification of released files.  However, this method should not be enabled by default and should be the exception not the norm. 

In the registry create the following DWORD (32-bit) value:

HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version 220\DEBUG\DOCMGMT_OVERRIDESTATUSCHECKFORFILEACCESS

Set this value to = 1.

Now, whenever you open a Released status file in Solid Edge, in the Read-Only Assistant window select "Request Check Out" and the file will immediately become modifiable without having to change the file status or creating a new revision:

If this method is to be used then a suggestion would be to consider implementing some sort of utility to quickly toggle this registry switch on and off as needed.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: DOC_MANAGEMENT

Ref: 002-8015592

KB Article ID# PL8015592

Contents

SummaryDetails

Associated Components