The default font has to be changed when creating a note for NX CAM Engraving.
Solution
Steps to creating a custom standard template for NX CAM:
- Go to 'File-->Utilities-->Customer Defaults'.

- Select 'Drafting-->General Setup'.

Note: The "Customize Drafting Standard - ISO" dialog is displayed.

- Select 'Common-->Lettering'.

- Select the 'Lettering' tab-->From "Text Parameters" group...type "yourdesiredfont" for the desired parameter. (Replace "yourdesiredfont" with the actual font needed.)
Note: You must know the exact name of the font...no dropdown is available

- Select "Save As" from the bottom right of the dialog box.

The "Save As Drafting Standard" dialog displays.

- Select "Apply" and Cancel the dialog box.
- Select 'Menu-->Tools-->Drafting Standard...'.

Note: The
"Standard" being used is displayed.

- Test the Default
- Select Application Drafting.
- Cancel when the "Sheet" dialog box is displayed.
- Select "Note" from the "Annotation" group on the "Ribbon".

- Select "Settings" from the "Note" dialog box.

The font default is now "blockfont".

Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V11.0.2
Function: PLANAR_MILLING
Ref: 002-8015573