Missing Simulation features from Solid Edge 2019 in Solid Edge 2020

2021-10-06T23:56:16Z

Summary


Details

If you have:

• Solid Edge Premium (SE388 Node locked/Floating)
• Solid Edge Simulation (SE385 Node locked/Floating)

You may have noticed that the Normal Modes/Buckling/Heat Transfer, is missing from the solutions in Solid Edge SE2020.

Solution

If you are an SE388 customer, the configuration of your product suite will be modified to add a new product called Solid Edge Simulation Legacy that will be at zero cost and zero maintenance charge for you. Solid Edge Simulation Legacy will contain all the simulation features that you had with SE 2019 and prior. This change will ensure that you continue to enjoy the simulation features with SE 2020 without incurring any additional cost.

If you are a SE385 customer, the configuration of your product suite will be modified to replace SE385 Solid Edge Simulation with SE387, Solid Edge Simulation Advanced - our new and enhanced product. 
The maintenance cost on SE387 is marginally higher than SE385, to reflect the higher value provided by SE387.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SIMULATION
Version: V220.0
Function: ENVIRONMENT

Ref: 001-8427372

KB Article ID# PL8015570

Contents

SummaryDetails

Associated Components