Solid Edge Cannot start Solid Edge Electrical Trial License server

2024-08-05T07:07:35Z
PART/SHEETMETAL SETUP

Summary


Details

I cannot start the SEE Trial license server. 

The system variable SEE_LICENSE_SERVER is set to 28000@hostname. 

Port 28000 is not blocked in the firewall.

Solution

Along with the SEE_LICENSE_SERVER=port@host the License Bundles environment variable also needs to be set:

SEE_LICENSE_BUNDLE=SEWIRHAR

Then stop the Services for the Electrical Manager and the Embedded Database, and then re-start from the Windows application menu instead.  Restarting the machine has also been known to resolve the problem.


Notes

If you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:

Solid Edge Portfolio Products Licensing FAQs Collection


KB Article ID# PL8015555

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES