I need to add a dependency to the rotating region so that the speed is not constant, to associate the speed of this rotating region with an objective searched for in the study - the torque.
With this I would get that the revolutions were not constant, but they will vary in function of the pair that is generating my real motor.
Solution
In FloEFD for a Dependency, the Goal dependency is only available for a Surface Source, Volume Source, Radiation Source, 2-Resistor Component, LED or TEC (see Help image below).
The Parameter Dependent Table specifies a dependency on one of the global EFD variables that can be defined in the Parameters feature (found in "Units - Parameters" of the FloEFD Command Bar).
The Parameters feature allows you to define parameters specifying their values and dimensions and then later using these parameters as global variables to create mathematical relationships or as simulation parameters within a Parametric Study.
The parameter can then be used in the Dependency of the Rotating Region definition, for example, using the table of values.
The Parameter variable can be used as the Simulation (or Parameter) item in the Parametric study which will, in turn, affect the rotating region dependency due to the table definition set above (the numbers are just entered as samples).
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: FLOEFD
Version: V220.0
Function: FLOEFD_SE
Ref: 001-9565882