Java Function Toolkit Licensing Issue

2021-10-07T00:08:41Z

Summary


Details

SFB Text
=========
 
Function toolkit based on Java fails with license error in Simcenter 3D 2019.2/NX 1872
 
Condition for problem to occur
-----------------------------------------
  1. Using Java Function toolkit
 
Java function toolkit changes were made in Simcenter 3D 2019.2/NX 1872 affecting the "afuapp.jar" file. The jar file has to be signed to avoid licensing issue.  Due to an oversight the jar file was not signed resulting in the function toolkit requiring license to launch
 
Affected Release
----------------
Simcenter 3D Response Dynamics 2019.2
 
Fixed Release
----------------
The issue is now fixed in Simcenter 3D Response Dynamics 2020.1. Additionally, Simcenter 2020.1 will have a native interface for function tools and will not be using Java interface

Contact Siemens GTAC support for further assistance if you are using Simcenter 3D 2019.2/NX 1872 version of the software
 
 

SFB-Simcenter-8015535
PR 9543022
Product Information:
  • Product: Simcenter
  • Product: NX , Application: CAE

KB Article ID# PL8015535

Contents

SummaryDetails

Associated Components