NX Objective is to move the object along the defined curve in defined time interval

2021-10-06T23:27:28Z
NX for Design

Summary


Details

Given the Time as an Input for the Path Constraint Joint which is 20 second. But this operation is finished in 1 second and after that the Drilling operation is happening.
I would like to know, why the Path constraint Joint operation finished in 1 second when I gave 20 second as an input? This will have an influence on the cycle time of the machine when more number of parts and sequences are added.

Solution

User need to modify the speed in the Position control and manage the overall time in comparison with 
Operation time duration, Operation time need to be sufficient to allow the operation to complete or the movement to complete and also can add idle time if needed.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: MECHATRONICS
Version: V12.0.2
Function: JOINT

Ref: 002-8015520

KB Article ID# PL8015520

Contents

SummaryDetails

Associated Components

Mechatronics Concept Designer