Dear Siemens PLM Customer,
We are pleased to inform you that the latest NX 1847 Series Critical Maintenance Software fix is now available for download from the Siemens PLM Download Server.
Please disregard this announcement if you are on the current NX 1872 Series.
Note: Automatic updates will not be available for releases on NX 1847 Series after NX 1867, including NX 1867.4400. Users who are on NX 1867 with the automatic update option turned on will be notified to download and install the next release on the NX 1872 Series. If NX 1867.4400 is preferred, users must download the release from the GTAC Download Server.
Download of NX on Windows 64-bit Please use the following steps to download the NX product release and its documentation.
Note: A valid
WebKey account is required.
- In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/
Login using your WebKey username and password
- From the Download page, enter "SiemensNX-1867.4400_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.
- Alternatively, the NX product release can be found using file navigator by entering NX into the Product Filter feature on the left of your browser and then navigating through the NX directory structure as follows:
- Expand the "NX Support" folder
- Expand the "NX Supported" folder
- Expand the "NX 1847 Series" folder
- Expand the current release folder (NX 1867.4400)
- To download the NX product:
- Right click on the Release Package file(s)
- Select "Save Target As" or "Save Link As" to save the file(s) to your local destination
- Note: There are two possible methods for downloading NX. The first approach is recommended for customers running any version of the NX 1847 Series (1847, 1851, 1855, 1859, 1863, or 1867) and would like to get the latest Critical Maintenance Software Fix for the NX 1847 Series. To upgrade, download the following file and double click to begin the installation program:
- SiemensNX-1867.4400_wntx64_MSP.zip
- The second approach is recommended for customers who may want to perform a complete install of the NX 1847 Series using this released Critical Maintenance Software Fix. The release can be downloaded as a single file:
- SiemensNX-1867.4400_wntx64.zip
- To download the NX documentation:
- Expand the "NX Support" folder
- Expand the "NX Supported" folder
- Expand the "NX 1847 Series" folder
- Expand the current release folder (NX 1867.4400)
- Expand the "Documentation" folder
- Right click on the product documentation link
- Select "Save Target As" or "Save Link As" to save the file to your local destination.
In all cases, please refer to the supplied README file for installation instructions.
If you encounter any problems during this installation, please contact your local Siemens PLM Software support office.
For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:
NX:
http://www.plm.automation.siemens.com/en_us/products/nx/ GTAC:
https://www.plm.automation.siemens.com/global/en/support/ Sincerely,
Siemens Product Lifecycle Management Software Inc.
Digital Factory Division
SFB-NX-8015505
Product Information: