Siemens PLM Licensing How can I know when a borrowed license will return to the server ?

2021-10-06T23:27:28Z
Licensing Maintenance

Summary


Details

When one or several users have borrowed licenses and are away, how do I know when these  licenses will be available on the server again ?



Solution

From a Windows command line, you can execute :

lmutil lmstat -a -c 28000@server_hostname

Look for the "linger" value which indicates the number of remaining seconds. You can then divide this value by 86400 (60 * 60 * 24) to get the number of days for this period length or by 3600 to get the number of hours.

For example :
    user1000 PC_client PC_client0.0 (v1.0) (licserver/28000 3201), start Thu 7/21 11:23  (linger: 345317 / 345540)

Remaining time = 345540 / 86400 = 4 days

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Function: SYSTEM_TOOLS

Ref: 002-8015457

KB Article ID# PL8015457

Contents

SummaryDetails

Associated Components

Siemens PLM Common Licensing