"Invalid digital signature"

2021-10-06T23:27:28Z

Summary


Details

During NX installation, the message "The program's digital signature is invalid" is displayed

Solution

Run: certmgr
 
 Check to see anything under the Trusted Root Certification Authorities tab?
 
 
 Is there a GlobalSign line with the Friendly Name of Google Trust Services - GlobalSign Root CA-R2 ?
 
 
 It is possible that the machine has a corrupted or missing root certificate store. 
Not sure how the machine does much if this is the case as root certificates are checked a lot in daily OS use.
 
 
 Info on configuring the trusted roots with a section on doing this on disconnected machines:

 https://docs.microsoft.com/en-us/previous-versions/windows/it-pro/windows-server-2012-R2-and-2012/dn265983(v=ws.11)




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1859
Function: WNT_INSTALL

Ref: 002-8015448

KB Article ID# PL8015448

Contents

SummaryDetails

Associated Components