NX Why "Publish JT Data" can not be selected if the part to be imported is selected first in the dialog?

2021-10-06T23:27:28Z
NX for Design

Summary


Details

"Publish JT Data" can not be selected if the part to be imported is selected first in the dialog.
Please tell me why "Publish JT Data" can not be selected.

Solution

"Publish JT Data" is possible only if the data is fully loaded in the import dialog, hence the decision of whether to load the data fully or partially in the import dialog has to be made upfront by selecting ON or OFF for "Publish JT Data" option.

Meaning:

When you open any assembly in NX you can load the assembly in Partial load or Fully Loaded mode, similarly same is applicable in the Import Dialog also.
"Publish JT Data" is only valid when data is fully loaded in the Import dialog.
The moment "Publish JT Data" option is ON data in Import dialog if fully loaded automatically.
The moment "Publish JT Data" option is OFF data in Import dialog if Partially loaded automatically.
Once the data is already loaded in the Import dialog these options cannot be switched.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: CLONE_IMPORT

Ref: 002-8015445

KB Article ID# PL8015445

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX