The variable radius points cannot be specified by % Arc Length of each edge

2021-10-06T23:27:28Z

Summary


Details

When multiple edges are selected in one list for Edge blend,


the variable radius point cannot be specified by "% Arc Length" of each edge.


However it was possible until NX10.



Solution

Base on the enhancement made in NX11.0.1, the calculation value of % Arc Length is according to the selected edge set (Not the Edge)


If you specify a variable radius bend point on a chain, NX now saves it as a percentage of the entire chain length, instead of the original curve or edge length.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V11.0.1
Function: FEATURE_MODEL

Ref: 002-8015439

KB Article ID# PL8015439

Contents

SummaryDetails

Associated Components