Details
Tool moves even when "Relocate Tool to Selection" is OFF in Transform Cage
When this option is turned off and select an object, the tool does not move.
However when additional objects are selected, the tool moves.
Solution
Though "Relocate Tool to Selection" is OFF, if "Reorient Tool to Selection" is ON and you select additional object, the transformer tool will be moved to the centroid of the selected objects and aligned with them.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: STUDIO_DESIGN
Version: V11.0.2
Function: SUBDIVISION
Ref: 002-8015437