NX What is the maximum number of expressions can be handled by "User Editable Expressions"?

2021-10-06T23:27:28Z
NX for Design

Summary


Details

What is the maximum number of expressions can be handled by "User Editable Expressions" of User Defined Feature Wizard?



Solution

The limit is depending on hardware/o/s and how many applications are currently running on that machine,  it is limited by the physics of that machine. The number is dynamic, but big enough for practical use



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V12.0.2
Function: FEATURE_MODEL

Ref: 002-8015436

KB Article ID# PL8015436

Contents

SummaryDetails

Associated Components

Modeling