Overstock can be placed directly on routing curve

2021-10-06T23:27:28Z

Summary


Details

Overstock can be placed directly on routing curve which is undesirable as there is no stock exists.


 
Steps


1) Create a routing curve


2) Place a pipe on routing line.


3) Place a overstock on pipe.


Overstock gets placed on pipe properly. But if there is no pipe and we try to place overstock directly on the routing curve, there also it gets placed, which is not desirable.


Can we restrict this behavior?



Solution

There is no way to restrict overstock placement when there is no stock(pipe) in current NX versions.


As per current design, the user is allowed to place stock(pipe) even after placing overstock as well.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ROUTING_GENERAL
Version: V12.0.2
Function: STOCK_AS_COMP

Ref: 002-8015435

KB Article ID# PL8015435

Contents

SummaryDetails

Associated Components