Customer default parameters for TAB feature are not working

2021-10-06T23:27:28Z

Summary


Details

Bend centerline /Bend Tangent line parameters are not reflecting in the TAB feature output. There is no difference in enabling or disabling these parameters.



Solution

The customer defaults settings for Bend centerline /Bend Tangent line are applicable only when using Multi Bend References in TAB feature.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NX_SHEET_METAL
Version: V12.0.1
Function: TAB

Ref: 002-8015434

KB Article ID# PL8015434

Contents

SummaryDetails

Associated Components