Slow response while editing a sketch of a work part using multiwindow

2021-10-06T23:27:27Z

Summary


Details

When editing a sketch of a work part in an assembly using a multi window, 


updating the current window slows the response of the screen display because other windows also getting updated. 



Solution

The cause of the delay is : 


When "Fixed Text Height on Screen" is ON, the sketch dimensions needs to update in the current screen and this change needs to be reflected in other windows as well.


If "Fixed Text Height on Screen" is set to OFF, the response is faster.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V12.0.2
Function: SKETCHER

Ref: 002-8015428

KB Article ID# PL8015428

Contents

SummaryDetails

Associated Components