NX Circular dependency detected when trying to unite several bodies

2021-10-06T23:27:27Z
NX for Design

Summary


Details

The user cannot unite several bodies using "Unite" command because of the following error


--------------------------------------------------------------------------


Circular dependency detected 


Did you try to modify the base body using something derived from an extracted or linked feature?


-----------------------------------------------------------------------------------



Solution

If you have any up-stream features like "Extracted face" or "Linked body" that has "Fix at Current Timestamp" checked OFF,  Please check it ON and try Unite which should solve the issue.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V11.0.1
Function: FEATURE_MODEL

Ref: 002-8015426

KB Article ID# PL8015426

Contents

SummaryDetails

Associated Components

Modeling