Translucency of Space Reservation is not retained

2021-10-06T23:27:27Z

Summary


Details

Translucency of Space Reservation is not retained.


 


Steps:


1.Change the Translucency of the body of the Space reservation from 50 to 0


2. Change the size of space reservation by moving a connected connector 


3. Notice that the translucency of the body returns to 50 



Solution

When you move the components, the stocks are recreated to match the shape change using the default space reservation stock Translucency value


Hence, Please set the following customer defaults value accordingly


File -> Utilities -> Customer Defaults -> Routing, General, Stock tab, "Space Reservation Stock Translucency", and change the value to 0%



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ROUTING_GENERAL
Version: V11.0
Function: LEGACY_STOCK

Ref: 002-8015425

KB Article ID# PL8015425

Contents

SummaryDetails

Associated Components