Details
User selects Tool position ON command before selecting the curve. But in New Planer mill interface, User is not able to predefine Tool position ON.
Solution
Currently this is designed behaviour.
In the old boundary dialog, it was not possible to define and edit the boundary and its members at the same time, which is why it was easy to allow for a "predefinition" of the tool side value which was then applied to the whole boundary as it was defined.
In the new dialog we have both parts - boundary selection and custom member data - available at the same time, which is why we need to clearly separate the data of these two.
Workaround: We have multiple edit for the members, so that it is possible to change the tool side values of all members at the same time.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1872
Function: PLANAR_MILLING
Ref: 002-8015423