Why turning does not recognize small Chamfers

2021-10-06T23:27:27Z

Summary


Details

Turning operation does not recognize small chamfers.

Solution

The issue is with after editing the Chamfer to "0.03" the chamfer feature missed from the "Part Spun Outline" if we see the Part Boundaries we can see 4 Members only.
 
So the operation missing the Chamfer.
 
The 'automatic' method of generating the spun outline can sometimes miss small features. The software is running up against the internal tolerance used to create the parasolid spun outline. 
 
The best work around for this situation is to use 'Planes at angles' instead of 'Automatic' for the turning work piece part spun outline. You often get a better approximation of the part boundary.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V1872
Function: TURNING

Ref: 002-8015421

KB Article ID# PL8015421

Contents

SummaryDetails

Associated Components