Details
When two different parts have same diameter holes, one hole is recognized as STEP HOLE and another hole is recognized as SLOT_ROUND. why?
Solution
If the cylinder covers more than half circle, then it lists as Step Hole (> 180 degrees).
If the cylinder covers less than half circle it lists as Slot Round ( <= 180 and > 90 degrees).
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V12.0.2
Function: FEATURE_BASED
Ref: 002-8015416