NX How to change "TCP_FIX_MACHINE" of SIM 15 to "TCP_FIX_TABLE

2021-10-06T23:27:27Z
NX for Manufacturing

Summary


Details

Which configuration file needs to be changed for converting "TCP_FIX_MACHINE" of SIM 15 to "TCP_FIX_TABLE"

Solution

PB_CMD_customize_output_mode is working with the OOTB SIM post only and it needs to be changed in the ini file.
 
For example in sim08_mill_5ax\cse_driver\fanuc , we need to change the sim08_mill_5ax_fanuc-Main.ini file
 


Current setting
(#19696=0 : rotating table coordinate system for G43.4/5. )

Change in INI program to 32 for non-rotating workpiece coordinate system
#19696=32
(This part sets the position of the reference point G28, G54)
G54
 
This is having connection with the driver file too.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V12.0.2
Function: LIBRARIES

Ref: 002-8015415

KB Article ID# PL8015415

Contents

SummaryDetails

Associated Components

Manufacturing General