NX The note of the Arial font is plotted in a character of the white space on a colored background

2021-10-06T23:27:27Z
NX System Administration

Summary


Details

 the character that I painted over when I make the explanatory note of the Arial font in NX.
However, it becomes the character of the white space on a colored background when it output it to an HPGL file.





Solution

The plotter profile is uses HPGL which produces wireframe outlined text. For filled text, use HPGL/2.






Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: GATEWAY
Function: PLOTTING

Ref: 002-8015410

KB Article ID# PL8015410

Contents

SummaryDetails

Associated Components

Plotting