Where used command not showing linked drafts of a model.

2021-10-06T23:56:13Z

Summary


Details

Where used command not showing linked drafts of a model even though the vault locations already updated in the FastSearchScope.txt in Solid Edge preferences folder. 
The 'BuiltinDiagApp.exe' doesn't work, system goes not responding.




Solution

Please follow below steps:
1.        Ensure that the vault should be completely indexed from Windows Indexing options.
2.        Restart the windows search service (and verify that it is configured to start automatically).
3.        Unregister and Register SEPropertyHandler.dll with administrator rights. For this -
Open Command Prompt with administrator rights. It should point to C:\windows\system32
    
-        To unregister, run command: regsvr32 <path to Solid Edge program folder>\SEPropertyHandler.dll -u
-        To register again, run command: regsvr32 <path to Solid Edge program folder>\SEPropertyHandler.dll
 



Notes and References

9541347

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEDM

Ref: 002-8015352

KB Article ID# PL8015352

Contents

SummaryDetails

Associated Components