Details
When trying to uninstall the Solid Edge Standard Parts administrator; it is showing an error as " Error: 1606. Could not access network location".
Solution
- The folder mentioned in the error message was not present at the specified location also the user was not having write access to the specified drive.
- Set the UAC (User account control) settings to Never Notify
- Turn OFF Windows Defender Firewall from Control panel > System and Securities
- Create (if deleted) or share (if not shared earlier) the remembered folder (mentioned in error message) temporarily and continue with uninstall process.
- Uninstall will continue after the old path is found.
Notes and References
9562282
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: INSTALL
Ref: 002-8015351