In Solid Edge SEDM mode the Open Draft command is not working.

2021-10-06T23:56:12Z

Summary


Details

In Solid Edge 2019 SEDM managed environment the 'Open draft' command returns with no drawing found message and does not opens the draft document. 

Solution

Please follow below procedure.
  • Ensure the vault location is added in the FastSearchscope.txt in Solid Edge Preferences folder
  • Ensure that the vault should be completely indexed from Windows Indexing options.
  • Run the 'BuiltinDiagApp.exe' from Solid Edge Program folder and validate.
  • Check if the Open Draft commend working or not
  • If the issue persist or the 'BuiltinDiagApp.exe' is not working, system goes to no response mode. Then try unregistering and reregistering the SEPropertyHandler.dll
 
Procedure:
1.        Restart the windows search service (and verify that it is configured to start automatically).
2.        Unregister and Register SEPropertyHandler.dll with administrator rights. For this -
Open Command Prompt with administrator rights. It should point to C:\windows\system32
    
-        To unregister, run command: regsvr32 <path to Solid Edge program folder>\SEPropertyHandler.dll -u
-        To register again, run command: regsvr32 <path to Solid Edge program folder>\SEPropertyHandler.dll
 



Notes and References

9534576

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: SEDM

Ref: 002-8015349

KB Article ID# PL8015349

Contents

SummaryDetails

Associated Components