August 19, 2019 Dear Solid Edge Customer: Solid Edge 2019 Maintenance Pack 9 is now available for download.
Sincerely,
The Solid Edge Team ============
Release Notes:============
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
=====================
Maintenance Pack Version:=====================
Solid Edge 2019 MP9
Version
: 219.00.09.04 ================
Download Location:================
Solid Edge 2019 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/ ==========
Installation:==========
- MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
- MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
- MSI Product Updates calculate free disk space before installing. Please be patient.
- MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
- MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
- Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
- When uninstalling, the original source media must be available to allow the recovery of previous file versions.
- The current MSI Product Update will be the only Update listed and available for uninstallation.
- After the current Product Update is uninstalled the previous Product Update will become the current Update.
- .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
===============
E-mail Notification: ===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
For details on initiating your email subscription navigate to:
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html ============================================
This Maintenance Pack addresses the following PRs:============================================
===API===PR 9528866: Solid Edge aborts when trying to get a plane or PMI plane from annotation object
PR 9541960: Styles standard COM enumerator can crash solid edge
PR 9541992: Windows standard enumerator can crash Solid Edge
===General===PR 9499888: Change SE status in Design Manager move files to the root folder in pre-release
PR 9511000: Wrong coordinate units with Probe command
PR 9503598: Update Status Info disabled with Solid Edge Foundation license
PR 9519306: A Total Bearing Load is being applied to each face with the total value.
PR 9542777: Common Views Window resizes when trying to move.
===Assembly=== PR 9324645: Unable to create chamfer assembly feature
PR 9362182: Unable to add Custom Occurrence Properties in some cases
PR 9426420: Assembly Move/Copy performance is slower compared to ST9
PR 9496664: Assembly that have features in them as being flagged as dirty on open
PR 9376294: Unable to run Piping Route utility (PreparePipingComponents.exe)
PR 9519529: Changing triad angle with Drag component command not working if angle typed in.
PR 9533162: Part geometry is wrong when zooming in and out
PR 9495996: Assembly: Editing sketch profile twice causes the document to go in error state
===Draft=== PR 9427462: Legacy parts list resets (turns on all) components in Options.
PR 9502972: Hidden callouts are not being located
PR 9498819: Changing "Terminator Type" will change at wrong end
PR 9524795: Crash placing view of AP asm after selecting FOA.
===Part/Profile/Sheet Metal===PR 9520457: Potential fix for a crashlog abort in the Sync interpart copy command
PR 9529624: Smart dimension with dimension axis is not driving.
PR 9518257: Under 'round' the blend command does not work in Shining 3D
PR 9530464: contour flange built with ST10 (or prior) fails when recomputed with 2019
PR 9531196: Crash doing move to sync on this part file.
PR 9537499: Access violation (trapped) when closing the FOP preview window
===Translators===PR 9487491: Crash while executing a 'Recompute' on a 'Part Copy' feature
PR 8732052: SW DATA MIGRATION wrong results
PR 9474274: SW2014 After the migration of the drawings are not the same
===Teamcenter Integration for Solid Edge===PR 9437078: Line of the L-Panel is updated incorrectly by executing Set "Save As Selected"
PR 9468700: Property of a part can only be updated once within an assembly
PR 9511650: Check - In and Revise of any 3D is failed when unexpected lines exist in MyHistory
PR 9512949: SEEC: props and .xml files not copied to Cache, "Object" displayed in Pathfinder
PR 9521479: "Auto Fit" always on by default
PR 9521797: Query that takes a long time to execute is performed by SESE operation
PR 8422144: SEEC Occurrence properties will not sync with TC find no for all FOA member
PR 9504722: CAM Express (NX12) is unable to open Solid Edge ST9 parts in TC 11.4.
PR 9418335: Overwriting another users work
PR 9498295: Script error during Check-In from Hosted AW
PR 9507704: User cannot change default UOM value on CPD.
===Mold Tooling===PR 9288728: Crash while exiting SE after closing mold and electrode project with "Close All"
===TechPub===PR 9344042: First time Save as of an assembly to QSM File cause components are incorrect
PR 9134662: Assembly display mode and zoom changes after export to QSM / Illustrations.
SFB-SOLID_EDGE-8015344
Product Information: