How to create an associative center of gravity point using the Measure command.
Solution
- In the Measure command dialog, select the Associative option in the Settings group as shown below.
- Select the solid body to be measured (the selection filter in the ribbon bar can be set to Solid Body).
- Once the body has been selected, expand the right side of the results display window by clicking on the right hand side of the boarder bar as shown below.
- Click on the basic curves icon in the display window for the Center of Gravity as shown below and click OK in the measure dialog.
- Change the rendering style to Static Wireframe to see the center of gravity symbol.
- Using Quick Pick by hovering over the center of gravity symbol, notice that an associative point has been created.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0
Function: INFO_ANALYSIS
Ref: 001-9560953