Pack and Go does not store assembly files correctly

2021-10-06T23:56:12Z

Summary


Details

Design Manager's Pack and Go does not appear to work correctly. The folder structure is not maintained although the setting "Maintain Folder Structure" was defined. The assembly files get stored at the wrong location. 

The Assembly data is located on a Network location which was added with "Map Network Drive" on the client system. 



Solution

This will cause the Design Manager's "Pack and Go" functionality to not maintain the Folder structure correctly.  Using "Add Network location" will maintain the folder structure. The destination folders and subfolders of the Assembly data will then be correctly created and files located to them.


Additional information: The Windows mapped drives technology dates back to Windows 3.1 and there are known issues with it.  Microsoft later introduced Universal Naming Convention (UNC) as a replacement to mapped drives with Add Network Location.  We recommend, especially with the use of the Design Manager, to setup the connection to the data with "Add network location" and the UNC Path.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1803
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP5
Function: DESIGN_MANAGER

Ref: 001-9432092

KB Article ID# PL8015311

Contents

SummaryDetails

Associated Components