Corresponding Standard Parts versions with Solid Edge
2021-10-06T23:57:52Z
Summary
Details
With each Solid Edge version we deliver Standard Parts. If no modifications have been made the version number does not change. Some Standard Parts need modifications either because the standard has changed or fixes were made for the parts. If so, then those new parts get new version numbers. The free content delivered when installing the Standard Parts Administrator with the option to install Master Parts has another version number to that of the parts delivered with the Machining or Piping Library.
Solution
These are the common version numbers:
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: SOLID_EDGE Application: APPLICATION Version: V221.0 Function: STANDARD_PARTS