How to remove newly displayed parts from an Illustration after a model update

2021-10-06T23:56:11Z

Summary


Details

How to remove newly displayed parts after a model update from Illustrations?  The advanced Select/Deselect Options no longer exist in Solid Edge 2020.



Solution

In Solid Edge 2020 the advanced select/deselect options are changed to simplify the handling. 

Now the advanced options are applied to currently selected Illustrations.  You will have to select the Illustrations, which should n–ot show the new parts after the model update, in the Storyboard. 
Select the required advanced option e.g. "Hide selected Parts" in the "Selected Illustrations" pulldown of the "Illustrate Ribbon/Storyboard Group".  This will remove the updated parts from the currently selected Illustrations



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: TECH_PUB
Version: V220.0
Function: ILLUSTRATIONS

Ref: 001-9557272

KB Article ID# PL8015288

Contents

SummaryDetails

Associated Components