Wrong Automatic Direction in turning operation

2021-10-06T23:27:26Z

Summary


Details

There are two identical FINISH_BORE Operation in a CAM-Setup.

In the first operation Automatic (CCLW) is enabled under Feeds and Speeds -> Direction


In the second operation only Automatic is shown.

The Direction should be Automatic (CCLW) as in the first operation




Solution

This behaviour is related to the Cut Region selection.

1. edit the second operation
2. edit Cut Regions
3. notice that Region Selection is set to "Specify", but there is no Point selected

4. set it to "Default" instead
5. generate the operation
6. check Feeds and Speeds
7. notice that the Direction is now Automatic (CCLW)


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: V12.0.2
Function: TURNING

Ref: 002-8015278

KB Article ID# PL8015278

Contents

SummaryDetails

Associated Components