Content Migration Manager - Drawings Will Not Migrate when Parts/Assemblies and Drawings are in the Same Teamcenter Item Revision

2021-10-07T00:08:40Z

Summary


Details

Issue
When attempting to migrate a drawing in a Teamcenter environment, drawings will not migrate if the part/assembly and the drawing are in the same Item Revision in Teamcenter. 

An error similar to the following occurs:
     "Failed to open part in function OpenBaseDisplay "
     "Failed to find dataset"
     "Failed to create NX Part"

The migration of the drawing does not complete and generates no results.

Solution:

An overlay to resolve this issue for the following Content Migration Manager (CMM) products can be found on the Siemens PL download center:   https://download.industrysoftware.automation.siemens.com/


     CMM for CATIA > Product Updates > V5 > NX Service:
          Readme.txt
          NXServiceDLLs1202mp12.7z
          NXServiceDLLs1202mp12.sha512.txt
          NXServiceDLLs1847.7z
          NXServiceDLLs1847.sha512.txt


     CMM for I-DEAS > Product Updates > NX Service:
          Readme.txt
          NXServiceDLLs1202mp12.7z
          NXServiceDLLs1202mp12.sha512.txt
          NXServiceDLLs1847.7z
          NXServiceDLLs1847.sha512.txt


     CMM for Pro/Engineer > Product Updates > NX Service:
          Readme.txt
          NXServiceDLLs1202mp12.7z
          NXServiceDLLs1202mp12.sha512.txt
          NXServiceDLLs1847.7z
          NXServiceDLLs1847.sha512.txt


     CMM for SolidWorks > Product Updates > NX Service:
          Readme.txt
          NXServiceDLLs1202mp12.7z
          NXServiceDLLs1202mp12.sha512.txt
          NXServiceDLLs1847.7z
          NXServiceDLLs1847.sha512.txt

Please  refer to the delivered Readme.txt for installation instructions

Workaround:
Migration can complete if the CMM Option for a drawing template is not provided.

SFB-NX-8015259
PR 9502569, 9516588
Product Information:
  • Product: NX

KB Article ID# PL8015259

Contents

SummaryDetails

Associated Components