NX Insert raster image into model is missing a degree of freedom for orientation compared to NX8.5

2021-10-06T23:27:26Z
NX for Design

Summary


Details

The new Raster Image dialog no longer contains the dynamic CSYS manipulator, as it did in the past.



Solution

In the Raster Image dialog, the workaround is to use the 'At Angle' plane constructor type during the Specify Plane step. This way, an extra rotational degree of freedom is available.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V12.0.2
Function: VISUALIZATION

Ref: 001-9554474

KB Article ID# PL8015238

Contents

SummaryDetails

Associated Components

Modeling