NX Step File export is exporting components residing on disabled layers in Data to Export tab

2021-10-06T23:27:26Z
NX for Design

Summary


Details

Disabling layers in the Data to Export tab in the Export to STEP Options dialog was being used in an attempt to prevent some components from being included in the STEP translation process, but these components were showing up when opening the STEP file. 



Solution

This is working as designed. Layer filtering is not supported at the component level. This is only supported at the part level or top assembly level.  A workaround for this case is to use suppression by arrangements in order to have control over which components are exported in the STEP translation. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V12.0.2
Function: STEP_AP214

Ref: 001-9554053

KB Article ID# PL8015226

Contents

SummaryDetails

Associated Components

CAD Translators