Is there some place I can find information on the use of Generative Design to obtain optimum results.
Solution
A link to example videos that will illustrate that if more definition is in the original model with design intent, you'll have more control over the Generative study result. The less definition in the model, the less control you'll have over the end result. The intent of Generative Design is to enhance a current design. Also massaging the model and the studies may be necessary to achieve the ultimate result.
https://www.gearupu.com/topology-optimization.htmlNotes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219MP7
Function: GENERATIVE_DSGN
Ref: 001-9551188