NC Output With ISV Machine Loaded (Post Builder)

2021-10-06T23:27:26Z

Summary


Details

The NC output with the ISV machine loaded is not the same as the NC output when the machine is not loaded.

Solution

  • Open the postprocessor in Post Builder.
  • Select Program & Tool Path --> Custom Command .
  • Scroll down and select the custom command... PB_CMD_reload_iks_parameters and place "return" and the top of the proc...as seen in the image below.


Notes and References

The solution is valid through the latest version of Post Builder... NX1876.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.2
Function: POSTBUILDER

Ref: 002-8015123

KB Article ID# PL8015123

Contents

SummaryDetails

Associated Components