Create Datum Plane on Body in Another Work Part, It Becomes Work Part.

2021-10-06T23:27:26Z

Summary


Details

NX12 and earlier with the assembly as the displayed part, a component the work part, create a datum plane on the solid body from another component within the assembly.


In NX1847 and later when selecting a face of the other non-workpart, that component then becomes the work part automatically and the datum is created in that part instead.

Solution

Added in NX1847 and later releases is the option:

'File -> Utilities -> Customer Defaults -> Modeling -> General (tab) -> Allow Automatic Work Part Change'


Change the default setting by unchecking it to work like NX12 and earlier releases of NX.


It is located at the bottom of the dialog (see image below).




NX11 and earlier Customer Defaults dialog



NX1847 and later Customer Defaults dialog


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: NX
Application: GATEWAY
Version: V1847
Function: CUSTOMER_DEFS

Ref: 002-8015067

KB Article ID# PL8015067

Contents

SummaryDetails

Associated Components