Error message returned when attempting to import the Solid Edge templates into Teamcenter

2021-10-06T23:56:06Z

Summary


Details

When attempting to import the Solid Edge templates to Teamcenter, getting the following error message: "An unexpected error occurred while importing the Solid Edge templates.  Correct the issue using the information captured in the log file and then import your templates."

Solution

This can occur if the Teamcenter preference, SEEC_ItemTypeList for Solid Edge files types does not include the item type of "Item" in the lists. 

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP4
Function: SEEC

Ref: 002-8015029

KB Article ID# PL8015029

Contents

SummaryDetails

Associated Components