Solid Edge The Validate command is returning no duplicate files information

2021-10-06T23:56:06Z
DOC_MANAGEMENT

Summary


Details

When performing a "Validate" command from the Common Properties dialog (CPd), Solid Edge is not finding duplicate files that are stored in the Solid Edge Data Management vault location.

Solution

 This behavior can occur if the indexing on the server has not completed, particularly for large file sets such as 1.5 million files in the vault.  Redefine the indexing to a smaller subset in the vault and the duplicates should be detected during the Validate.  

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 2012_R2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP6
Function: SEDM

Ref: 002-8015027

KB Article ID# PL8015027

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: OTHER