Solid Edge Error returned when attempting to create a new Solid Edge file in Solid Edge Embedded Client

2021-10-06T23:56:05Z
DOC_MANAGEMENT

Summary


Details

When attempting to create a new Solid Edge file the following error message was presented when the template dialog displayed:
"All Teamcenter FMS servers are unavailable. Contact your Teamcenter Administrator to correct this issue. This Save is queued and will retry on your next Teamcenter activity. If you cancel this action, the Data set in Teamcenter will not have a document. FMS was unable to provide the requested document. Validate that FMS is configured and operational, check your Teamcenter Volume(s) and then validate permissions to these Volume(s)".

Solution

This will occur if the Solid Edge templates folder in Teamcenter contains items that were uploaded by multiple users. 

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP9
Function: SEEC

Ref: 002-8015025

KB Article ID# PL8015025

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC