Insight Migration tool is not extracting AutoCad files saved in Sharepoint

2021-10-06T23:56:05Z

Summary


Details

Running the new Insight Migration Tool is not extracting AutoCAD files from the SharePoint database.  

Solution

The AutoCAD files need to be added to SharePoint using a Solid Edge tool in order for this to work so that the associated Solid Edge Mandatory Properties are added to files.  These properties are keyed on during the extract process, so if they are not there, the files are ignored.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: SOLID_EDGE
Application: APPLICATION
Version: V219MP8
Function: NONE

Ref: 002-8015023

KB Article ID# PL8015023

Contents

SummaryDetails

Associated Components