The NX customer default UGMGR_SeedPartName not found

2022-10-24T10:25:12Z

Summary


Details

When loading an item revision without UGMaster dataset into NX, NX is outputting the following error message:

"The NX customer default UGMGR_SeedPartName specifies a title which does not exist in Teamcenter. Because of this, all the seed parts will be set to the default one."

Examine the Customer Defaults setting at Teamcenter Integration > General > Parts Without NX Datasets tab:

Display Seed Part Dialog Box = No

Default seed Part = custom_Inch (also tried the OOTB "Metric" and "Inch"

Regardless what the value is set to, all result in above error. 

It has been confirmed these seed parts: custom_Inch, Metric, and Inch all resides under infodba:Unigraphics seed parts folder, and it is the Item Name that is appearing in the Customer Defaults value. 

Why is this not working?

Solution

This can be caused by different values in the different levels of customer defaults; make sure to check that setting value in all different levels of customer defaults. A lower level customer defaults may have an incorrect value and is not locked down by the higher level customer defaults with a correct value.

Notes

Notes

KB Article ID# PL8015006

Contents

SummaryDetails

Associated Components