NX Start NX via startup batch file, NX Viewer (or other application) gets started

2021-10-06T23:27:25Z
NX System Administration

Summary


Details

Start NX via startup batch file, NX Viewer (or other application) gets started

Solution

In the startup script NX gets started via "C:\...\NX11\NXBIN\ugraf.exe".


If the "-nx" parameter is omitted, NX will start with the last used application.
To make sure that main NX is started, add the "-nx" parameter at the end :
"C:\...\NX11\NXBIN\ugraf.exe -nx".



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: SYSENG
Version: V11.0
Function: INSTALL_ISSUES

Ref: 002-8014984

KB Article ID# PL8014984

Contents

SummaryDetails

Associated Components

Installation