Details
Customized Parts List has all table lines in Green, with a line width of 0.13 mm. and text font in Red, some of these lines turn into Dark Blue with a line width of 0.18 mm. after this template has been dragged into the drawing, text of added lines turns back to black.
Solution
When selecting the entire Parts List, change the cell line settings, text, etc. and save it as a template, it goes wrong.
But when selecting column by column, change the cell line settings, text, etc. and save it as a template, then the Parts List template works properly.
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: DRAFTING
Version: V9.0
Function: TABLES
Ref: 002-8014982